PLTransportLayer.ShaftEncoderModeEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.ShaftEncoderModeEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLTransportLayer.ShaftEncoderModeEnum | Initializes a new instance of the PLTransportLayer.ShaftEncoderModeEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | FilterX1 | Shaft encoder mode is set to X1. Applies to: CoaXPress |
![]() | FilterX2 | Shaft encoder mode is set to X2. Applies to: CoaXPress |
![]() | FilterX4 | Shaft encoder mode is set to X4. Applies to: CoaXPress |
![]() | Name | The full name of ShaftEncoderMode (Overrides ParameterListEnum.Name.) |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of ShaftEncoderMode (Overrides Object.ToString()()()().) |
PLTransportLayer.ShaftEncoderModeEnum.ToString Method#
The full name of ShaftEncoderMode
Return Value#
Type: String
Returns the full name of ShaftEncoderMode
PLTransportLayer.ShaftEncoderModeEnum Constructor#
Initializes a new instance of the PLTransportLayer.ShaftEncoderModeEnum class
PLTransportLayer.ShaftEncoderModeEnum.FilterX1 Property#
Shaft encoder mode is set to X1.
Applies to: CoaXPress
PLTransportLayer.ShaftEncoderModeEnum.FilterX2 Property#
Shaft encoder mode is set to X2.
Applies to: CoaXPress
PLTransportLayer.ShaftEncoderModeEnum.FilterX4 Property#
Shaft encoder mode is set to X4.
Applies to: CoaXPress
PLTransportLayer.ShaftEncoderModeEnum.Name Property#
The full name of ShaftEncoderMode