PLTransportLayer.TriggerInSourceEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerInSourceEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLTransportLayer.TriggerInSourceEnum | Initializes a new instance of the PLTransportLayer.TriggerInSourceEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | GPITriggerSource0 | Trigger Source is set to GPI 0. Applies to: CoaXPress |
![]() | GPITriggerSource1 | Trigger Source is set to GPI 1. Applies to: CoaXPress |
![]() | GPITriggerSource2 | Trigger Source is set to GPI 2. Applies to: CoaXPress |
![]() | GPITriggerSource3 | Trigger Source is set to GPI 3. Applies to: CoaXPress |
![]() | GPITriggerSource4 | Trigger Source is set to GPI 4. Not available on LightBridge. Applies to: CoaXPress |
![]() | GPITriggerSource5 | Trigger Source is set to GPI 5. Not available on LightBridge. Applies to: CoaXPress |
![]() | GPITriggerSource6 | Trigger Source is set to GPI 6. Not available on LightBridge. Applies to: CoaXPress |
![]() | GPITriggerSource7 | Trigger Source is set to GPI 7. Not available on LightBridge. Applies to: CoaXPress |
![]() | Name | The full name of TriggerInSource (Overrides ParameterListEnum.Name.) |
![]() | TriggerInSourceFrontGPI0 | The trigger input source is set to TriggerInSourceFrontGPI0. Applies to: CoaXPress |
![]() | TriggerInSourceFrontGPI1 | The trigger input source is set to TriggerInSourceFrontGPI1. Applies to: CoaXPress |
![]() | TriggerInSourceFrontGPI2 | The trigger input source is set to TriggerInSourceFrontGPI2. Applies to: CoaXPress |
![]() | TriggerInSourceFrontGPI3 | The trigger input source is set to TriggerInSourceFrontGPI3. Applies to: CoaXPress |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of TriggerInSource (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerInSourceEnum.ToString Method#
The full name of TriggerInSource
Return Value#
Type: String
Returns the full name of TriggerInSource
PLTransportLayer.TriggerInSourceEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerInSourceEnum class
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource0 Property#
Trigger Source is set to GPI 0.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource1 Property#
Trigger Source is set to GPI 1.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource2 Property#
Trigger Source is set to GPI 2.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource3 Property#
Trigger Source is set to GPI 3.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource4 Property#
Trigger Source is set to GPI 4. Not available on LightBridge.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource5 Property#
Trigger Source is set to GPI 5. Not available on LightBridge.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource6 Property#
Trigger Source is set to GPI 6. Not available on LightBridge.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource7 Property#
Trigger Source is set to GPI 7. Not available on LightBridge.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.Name Property#
The full name of TriggerInSource
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI0 Property#
The trigger input source is set to TriggerInSourceFrontGPI0.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI1 Property#
The trigger input source is set to TriggerInSourceFrontGPI1.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI2 Property#
The trigger input source is set to TriggerInSourceFrontGPI2.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI3 Property#
The trigger input source is set to TriggerInSourceFrontGPI3.
Applies to: CoaXPress