跳转到内容
STAGING SERVER
DEVELOPMENT SERVER

故障排除#

问题:未检测到相机#

Issue: The camera doesn't appear in the camera list or can't be opened.

Solution:

  • Verify the USB Type-C cable is properly connected to the camera.
  • Try a different USB port (preferably USB 3.0) and a different USB cable.
  • Check Device Manager for the camera device. If there's an unknown device, install the latest pylon SDK drivers.
  • Ensure the pylon SDK is properly installed.
  • Try unplugging and reconnecting the camera.

Issue: The camera doesn't appear in the camera list or can't be opened.

Solution:

  • Verify the USB Type-C cable is properly connected to the camera.
  • Try a different USB port (preferably USB 3.0) and a different USB cable.
  • Verify the camera is detected: lsusb | grep Basler
  • Ensure the pylon SDK is properly installed. Verify with which pylon.
  • Try unplugging and reconnecting the camera.

Issue: The camera doesn't appear in the camera list or can't be opened.

Solution:

  • Verify the USB Type-C cable is properly connected to the camera.
  • Try a different USB port (preferably USB 3.0) and a different USB cable.
  • Verify the camera is detected: lsusb | grep Basler
  • Ensure the pylon SDK is properly installed. Verify with which pylon.
  • Try unplugging and reconnecting the camera.

问题:图像 Quality 较差#

问题:图像出现噪点、过暗或模糊。

解决方案:

  • 调整曝光,例如:

    camera.ExposureAuto.SetValue(ExposureAuto_Continuous)
    
  • 确保照明充足。如有必要,请降低背光。对于采用主动立体视觉的 Stereo mini 相机,请确保环境光不过强。

  • 选择针对您的用例优化的深度预设。
  • 用软布清洁镜头,并确保已取下镜头盖。

问题:深度数据问题#

问题:深度数据无效、稀疏或不准确。

解决方案:

  • 确保场景中具有足够的纹理。
  • 对于主动立体相机(STM-502u、STM-952u),如有必要,请减小环境光。
  • 避免正对着相机的强反光表面。
  • 选择针对您的用例优化的深度预设。

问题:性能优化#

问题:采集或处理速度慢或资源消耗大。

解决方案:

  • 使用合适的采集策略,例如:

    camera.StartGrabbing(pylon.GrabStrategy_LatestImageOnly)  # For real-time
    
  • 尽可能使用原生格式处理图像,并为您的应用使用高效的算法。

  • 检查 CPU 使用率、Memory 消耗和 USB 带宽使用情况。

问题:OpenCV 的 DLL 或依赖项问题#

Issue: The code execution cannot proceed because opencv_core.dll was not found.

Solution: Add the folder containing the OpenCV DLLs to your PATH environment variable.

See Adding OpenCV to PATH Environment Variable in the C++ Programmer's Guide.

Issue: opencv_core.so: cannot open shared object file.

Solution: Make sure OpenCV is properly installed and the library path is added to LD_LIBRARY_PATH.

Issue: opencv_core.so: cannot open shared object file.

Solution: Make sure OpenCV is properly installed and the library path is added to LD_LIBRARY_PATH.

问题:PCL 的 DLL 或依赖项问题#

Issue: The code execution cannot proceed because OpenNI2.dll was not found.

Solution: Download OpenNI2 and add the folder containing the OpenNI2.dll to your PATH environment variable.

Issue: OpenNI2.so: cannot open shared object file.

Solution: Install the required OpenNI2 library package.

Issue: OpenNI2.so: cannot open shared object file.

Solution: Install the required OpenNI2 library package.

问题:PCL 的 CMake 配置错误 (RelWithDebInfo)#

Issue: When compiling a program that uses PCL with cmake, an error message similar to Compiler: C++ compiler determination failed occurs.

Solution: When building PCL in the CMake GUI, use the Release configuration instead of RelWithDebInfo.

Issue: PCL compilation problems.

Solution: Use the libpcl-dev package instead of building from source.

Issue: PCL compilation problems.

Solution: Use the distribution's PCL package if available, or build from source with Release configuration.

问题:混合使用 32 位和 64 位库#

问题:混合使用 32 位和 64 位库时出现链接器错误。

解决方案:确保所有库(pylon、OpenCV、PCL)均针对与您的应用程序相同的架构进行编译(全部为 32 位或全部为 64 位)。

问题:Debug 模式下帧率低#

问题:与 Release 模式相比,在 Debug 模式下运行时的帧率明显较低。

解决方案:这是正常现象。请在 Release 模式下编译以获得更好的性能。Debug 模式具有额外的开销。

问题:设备已连接错误#

问题: 在发生崩溃或程序异常终止后,应用程序无法连接到设备,因为其报告 Device already in use.

解决方案:

  • 重启 pylon 运行时或重新启动系统。
  • 检查是否还有其他进程仍在保持与该设备的连接。