Operator Library: Filter
运算符 MIN 用于识别并输出输入内核数据流的最小值。 该最小值将从 O 端输出。 该运算符不会输出最小值的内核索引。
| Link Parameter | Input Link I | Output Link O |
|---|---|---|
| Bit Width | [1, 64] 无符号,[2, 64] 有符号 | as I |
| Arithmetic | {unsigned, signed} | as I |
| Parallelism | any | as I |
| Kernel Columns | any | 1 |
| Kernel Rows | any | 1 |
| Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as I |
| Color Format | VAF_GRAY | as I |
| Color Flavor | FL_NONE | as I |
| Max. Img Width | any | as I |
| Max. Img Height | any | as I |

上一页