Operator Library: Logic
算子 XOR 执行按位逻辑 XOR(异或)操作。
如果相应输入位值的总和为奇数,则每个输出位设置为逻辑“1”,否则输出为
“0”。
必须在实例化模块时选择输入 link 的数量。
因此,具有 n 个输入的输出位 i 为
| Property |
值 |
| Operator Type |
O |
|
输入链路
|
I0,数据输入 I1..In-1,数据输入
|
|
Output Link
|
O,数据输出 |
| Link Parameter |
输入链接 I0 |
输入链接 I1..In-1 |
Output Link O |
| Bit Width |
[1, 64] |
as I |
as I |
| Arithmetic |
{unsigned, signed} |
as I |
as I |
| Parallelism |
any |
as I |
as I |
| Kernel Columns |
any |
as I |
as I |
| Kernel Rows |
any |
as I |
as I |
| Img Protocol |
{VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D, VALT_SIGNAL} |
as I |
as I |
| Color Format |
any |
as I |
as I |
| Color Flavor |
any |
as I |
as I |
| Max. Img Width |
any |
as I |
as I |
| Max. Img Height |
any |
as I |
as I |
|
|
对于无符号值,输入 Bit Width 的范围是 [1, 64]。
对于有符号输入,范围是 [2, 64]。
对于无符号彩色输入,范围是 [3, 63],对于有符号彩色,范围是 [6, 63]。
|